Hi,
Using an ACIM motor, I'm trying to smoothly transition from V/Hz scaler mode to velocity control using FAST.
In V/Hz mode Vq is set and the angle is manually incremented. Then V/Hz mode is exited and SPINTAC velocity control takes over. I've tried keeping SpinTAC velocity control disabled until V/Hz mode is exited, or when V/Hz is exited setting initial values of Iq in SPINTAC with STVELCTL_setTorqueReference(). So far everything I have tried results in the iq reference changing quickly at the switch point and sometimes even going negative, and the speed overshooting drastically.
What are the keys to transition from V/Hz to FAST with velocity control?
Thanks.