This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"error disconnecting from target" while build and executing on TMS320f28335 using MATLAB



Hello,

I am testing a four pulse generators in simulink on different GPIOs and wanted run on 28335 dock. while the building the process the output is fine but at last matlab trying to disconnect the dsp and it fails.

C:\Users\vinod\Desktop\flash test\untitled_ert_rtw>exit /B 0
"### Invoking postbuild tool "Download" ..."
C:/ti/ccsv5/ccs_base/SCRIPT~1/bin/dss.bat C:\PROGRA~1\MATLAB\R2013b/toolbox/idelink/EXTENS~1/ticcs/ccsdemos/RUNPRO~1.JS C:\MATLAB\SUPPOR~1\R2013b\tic2000/CCS_CO~1/F28335~1.CCX ../untitled.out
*** User inputs:
Target Configuration: C:\MATLAB\SUPPOR~1\R2013b\tic2000/CCS_CO~1/F28335~1.CCX
Program Name: ../untitled.out
Board Name: unspecified (connect to first board)
CPU Name: unspecified (connect to first CPU)
*** Starting debug session...
*** Debug Session Name: Texas Instruments XDS100v1 USB Emulator_0/C28xx
*** Board Name: Texas Instruments XDS100v1 USB Emulator_0
*** CPU Name: C28xx

*** Connecting to target...
*** Loading the program to the target...
*** Program is running.

*** Disconnecting from target...
SEVERE: Timed out after 90000ms
SEVERE: Error disconnecting from the target: Timed out after 90000ms

*** Terminating debug session...

after this nothing is happening but the output is fine.... now if I unplug the usb, only the first GPIO (34) is giving some random pulses and the other pins are just HIGH.