Other Parts Discussed in Thread: CONTROLSUITE
I was trying to debug a recieve interrupt that was never running for SCI-A, and tracked the problem back to the RX pin itself (GPIO28). The device communicating with the F28335 has a maximum current of 2mA on its serial lines, and the voltage is only varying between 1.85V and 3.3V.
Using SCI-B (GPIO 15), this problem does not occur; the 2mA is sufficient to vary the line voltage between 0 and 3.3V and the recieve interrupt is called as expected.
In both cases, I commanded the pull-up resistors to be disabled, but on the command
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1;
GPIO 28 goes high (and puts out a lot of current to stay high) while
GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 2;
leaves GPIO 15 low.
Do I have a defective board? Or is there something I overlooked that will make SCI-A work correctly?
code:
//-------------------------------------------------------------------------------------------------------------------------
#include "include/DSP2833x_Device.h" // Device Headerfile and Examples Include File
#include "include/DSP2833x_Examples.h" // DSP2833x Examples Include File
#define SCIPORT 0//0=A, 1=B, 2=C
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 9500//100E3
#define SCI_PRD LSPCLK_FREQ/8/SCI_FREQ-1
interrupt void sciTxIsr(void);
interrupt void sciRxIsr(void);
// Global variables
struct SCI_REGS *thisSci;
char txBuffer[]="Hello World!\0\0";
char rxBuffer[16];// Received data
void main(void){
InitSysCtrl();// PLL, WatchDog, enable Peripheral Clocks
DINT;// Disable CPU interrupts
IER = 0x0000;// Disable CPU interrupts
IFR = 0x0000;// clear all CPU interrupt flags
InitPieCtrl();// Initialize PIE control registers (all PIE interrupts disabled and flags cleared; DSP2833x_PieCtrl.c)
InitPieVectTable();// Initialize the PIE vector table with pointers to the shell Interrupt Service Routines (found in DSP2833x_DefaultIsr.c) DSP2833x_PieVect.c
EALLOW; // This is needed to write to EALLOW protected registers
#if SCIPORT==0
PieVectTable.SCIRXINTA = &sciRxIsr;// Interrupts are re-mapped to ISR functions
PieVectTable.SCITXINTA = &sciTxIsr;// Interrupts are re-mapped to ISR functions
#elif SCIPORT==1
PieVectTable.SCIRXINTB = &sciRxIsr;// Interrupts are re-mapped to ISR functions
PieVectTable.SCITXINTB = &sciTxIsr;// Interrupts are re-mapped to ISR functions
#elif SCIPORT==2
PieVectTable.SCIRXINTC = &sciRxIsr;// Interrupts are re-mapped to ISR functions
PieVectTable.SCITXINTC = &sciTxIsr;// Interrupts are re-mapped to ISR functions
#endif
//--- Group A pins
GpioCtrlRegs.GPACTRL.all = 0x00000000; // QUALPRD = SYSCLKOUT for all group A GPIO
GpioCtrlRegs.GPAQSEL1.all = 0x00000000; // No qualification for all group A GPIO 0-15
GpioCtrlRegs.GPAQSEL2.all = 0x00000000; // No qualification for all group A GPIO 16-31
GpioCtrlRegs.GPADIR.all = 0xFFFFFFFF; // All group A GPIO are outputs
GpioCtrlRegs.GPAPUD.all = 0xFFFFFFFF; // Pullups disabled
GpioCtrlRegs.GPAMUX1.all= 0x00000000;
GpioCtrlRegs.GPAMUX2.all= 0x00000000;
GpioCtrlRegs.GPBCTRL.all = 0x00000000; // QUALPRD = SYSCLKOUT for all group B GPIO
GpioCtrlRegs.GPBQSEL1.all = 0x00000000; // No qualification for all group B GPIO 32-47
GpioCtrlRegs.GPBQSEL2.all = 0x00000000; // No qualification for all group B GPIO 48-63
GpioCtrlRegs.GPBDIR.all = 0xFFFFFFFF; // All group B GPIO are outputs
GpioCtrlRegs.GPBPUD.all = 0xFFFFFFFF; // Pullups disabled
GpioCtrlRegs.GPBMUX1.all= 0x00000000;
GpioCtrlRegs.GPBMUX2.all= 0x00000000;
EDIS; // This is needed to disable write to EALLOW protected registers
GpioDataRegs.GPACLEAR.all=0xFFFFFFFF;//zero GPIO pins 0-31
GpioDataRegs.GPBCLEAR.all=0xFFFFFFFF;//zero GPIO pins 32-63
EALLOW;
#if SCIPORT==0
GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (SCIRXDA)
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // Configure GPIO28 for SCIRXDA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // Configure GPIO29 for SCITXDA operation*/
/*GpioCtrlRegs.GPBQSEL1.bit.GPIO36 = 3; // Asynch input GPIO28 (SCIRXDA)
GpioCtrlRegs.GPBMUX1.bit.GPIO36 = 1; // Configure GPIO28 for SCIRXDA operation
GpioCtrlRegs.GPBMUX1.bit.GPIO35 = 1; // Configure GPIO29 for SCITXDA operation*/
#elif SCIPORT==1
GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3; // Asynch input GPIO15 (SCIRXDC)
GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 2; // Configure GPIO15 for SCIRXDC operation
GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 2; // Configure GPIO14 for SCITXDC operation*/
/*GpioCtrlRegs.GPAQSEL2.bit.GPIO23 = 3; // Asynch input GPIO15 (SCIRXDC)
GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 3; // Configure GPIO15 for SCIRXDC operation
GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 3; // Configure GPIO14 for SCITXDC operation*/
#elif SCIPORT==2
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // Asynch input GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 1; // Configure GPIO62 for SCIRXDC operation
GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation*/
#endif
EDIS;
#if SCIPORT==0
thisSci=(struct SCI_REGS*)&SciaRegs;
#elif SCIPORT==1
thisSci=(struct SCI_REGS*)&ScibRegs;
#elif SCIPORT==2
thisSci=(struct SCI_REGS*)&ScicRegs;
#endif
thisSci->SCICCR.all =0x0007; // 8N1 No loopback, async mode, idle-line protocol
thisSci->SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, Disable RX ERR, SLEEP, TXWAKE
thisSci->SCICTL2.bit.TXINTENA =1;
thisSci->SCICTL2.bit.RXBKINTENA =1;
thisSci->SCIHBAUD = (long)(SCI_PRD) >> 8;
thisSci->SCILBAUD = (long)(SCI_PRD) & 0xFF;
//thisSci->SCICCR.bit.LOOPBKENA =1; // Enable loop back
thisSci->SCICTL1.all =0x0023; // Relinquish SCI from Reset
// Enable interrupts required for this example
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
#if SCIPORT==0
PieCtrlRegs.PIEIER9.bit.INTx1=1; // PIE Group 9, INT1; SCIRXINTA
PieCtrlRegs.PIEIER9.bit.INTx2=1; // PIE Group 9, INT2; SCITXINTA
#elif SCIPORT==1
PieCtrlRegs.PIEIER9.bit.INTx3=1; // PIE Group 9, INT3; SCIRXINTB
PieCtrlRegs.PIEIER9.bit.INTx4=1; // PIE Group 9, INT4; SCITXINTB
#elif SCIPORT==2
PieCtrlRegs.PIEIER8.bit.INTx5=1; // PIE Group 8, INT5; SCIRXINTC
PieCtrlRegs.PIEIER8.bit.INTx6=1; // PIE Group 8, INT6; SCITXINTC
#endif
IER = 0x100; // Enable CPU INT
EINT;// Enable CPU INT
thisSci->SCITXBUF=0;//trigger SCITXINTA
for(;;);// Step 6. IDLE loop. Just sit and loop forever
}
interrupt void sciTxIsr(void){
static Uint32 ii=0;
thisSci->SCITXBUF=txBuffer[ii++]; // Send data
if(ii >= sizeof(txBuffer)){
for(ii=0;ii<50*65535;ii++);
ii = 0;
}
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
interrupt void sciRxIsr(void){
static Uint16 ii=0;
rxBuffer[ii++] = thisSci->SCIRXBUF.all; // Read data
if(ii >= sizeof(rxBuffer))
ii = 0;
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
//===========================================================================
// End of code
//===========================================================================