Hi,
We need advice in selecting C2000 device for a Solar application with Arc Detection.
Is it possible to implement a Solar application with a single C2000 MCU
which includes Inverter control as well as Arc Detection.
The White paper mentions that Piccolo could be used for Arc Detection,
but if want to control the complete application should we opt for high end Delphino like F28377D?
We need your advice from which device should we start the evaluation.
And if possible please let us know what could be the software structure
if we try to implement this on a single MCU.
Best Regards
Kummi