Hello,
I am trying to work with the CLA module of a C2000 Microcontroller(F28069) in Simulink. If I have a Constant Block in the CLA Task Subsystem I get an error:
"cla_task.cla", line 33: error: identifier "modelname_t_P" is undefined 1 error detected in the compilation of "cla_task.cla".
I then checked the CLA Blinking LED Example, because there is a Constant Block in use, and the Example is compiling without problem. After Comparing the two generated cla_task.cla files I see a big difference. In the Example the Constant Block was put in with its value, while in my case, the Constant Block was put in as an element of a structur(modelname_t_P.Constant_Value), but this struct is not defined in the generated code.
I compared both Model Configurations, but couldn't find a difference. Can somebody tell me what I have to do, so I can use a Constant Block in a CLA Task Subsystem? I am using MATLAB 2015b and CCS v6.
Thank you for your support.
Kind Regards
Martin