Hello everyone,
I am using the 28335 delfino and struggle to get the Digital Controller Library running. I consulted the user guide (SPRUI31) which on page 15 and 16 describes how to add the DCL to my code.
In particular, step #3 on page 16 gives me headache as I have no real experience with the linker command file as for now (and consequently struggle to find the proper information in the SPRU513 documentation). In particular, step #3 says:
"...C28x library functions are placed in the user-defined code section “dclfuncs”. An example showing how this section might be mapped into the internal L4 RAM memory block is shown below:
dclfuncs : > RAML4, PAGE = 0
..."
When I look at the 28335_RAM_Ink.cmd linker command file, there is no such thing as dclfuncs. The same applies to the DSP2833x_Headers_nonBIOS.cmd linker command file.
I would appreciate it if you could guide me in this matter.
Please find a screenshot of where I currently am, as well as the C code of my current project.
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include <math.h> #include "DCL.h" // Header file for digital control purposes // Prototype statements for functions found within this file. void InitEPwm2(void); void InitializeADC(void); __interrupt void adc_isr(void); // User defined double PRD; #define RESULTS_BUFFER_SIZE 256 //buffer for storing conversion results Uint16 AdcaResults[RESULTS_BUFFER_SIZE]; Uint16 resultsIndex; volatile Uint16 bufferFull; float uk; // control PI pi1 = PI_DEFAULTS; void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xS_SysCtrl.c file. InitSysCtrl(); // Setting the controller gains pi1.Kp = 2200.0f; pi1.Ki = 0.002f; // Define ADCCLK clock frequency ( less than or equal to 25 MHz ) // Assuming InitSysCtrl() has set SYSCLKOUT to 150 MHz EALLOW; SysCtrlRegs.HISPCP.all = 3; EDIS; // Step 2. Initialize GPIO: // This example function is found in the F2837xS_Gpio.c file and // illustrates how to set the GPIO to its default state. InitGpio(); // For this case just init GPIO pins for ePWM1, ePWM2, ePWM3 // These functions are in the F2837xS_EPwm.c file InitEPwm2Gpio(); InitAdc(); // For this example, init the ADC // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xS_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2837xS_DefaultIsr.c. // This function is found in F2837xS_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers // PieVectTable.EPWM2_INT = &epwm2_isr; //function for ePWM2 interrupt PieVectTable.ADCINT = &adc_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize the Device Peripherals: // For this example, only initialize the ePWM and ADC EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; InitEPwm2(); InitializeADC(); //Initialize results buffer for(resultsIndex = 0; resultsIndex < RESULTS_BUFFER_SIZE; resultsIndex++) { AdcaResults[resultsIndex] = 0; } resultsIndex = 0; bufferFull = 0; EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC =1; EDIS; // Enable ADCINT in PIE PieCtrlRegs.PIEIER1.bit.INTx6 = 1; IER |= M_INT1; // Enable CPU Interrupt 1 EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Step 6. IDLE loop. Just sit and loop forever (optional): //take conversions indefinitely in loop do { //wait while ePWM causes ADC conversions, which then cause interrupts, //which fill the results buffer, eventually setting the bufferFull //flag while(!bufferFull); bufferFull = 0; //clear the buffer full flag }while(1); } /* Interrupt service routine reading the output voltage and generating the PWM */ __interrupt void adc_isr(void) { AdcaResults[resultsIndex++] = AdcRegs.ADCRESULT0 >>4; if(RESULTS_BUFFER_SIZE <= resultsIndex) { resultsIndex = 0; bufferFull = 1; } uk = DCL_runPI(&pi1, 0xC28, AdcaResults[resultsIndex++]); // Generates the new duty cycle EPwm2Regs.CMPA.half.CMPA=uk; // Reinitialize for next ADC sequence AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1 AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE } void InitEPwm2() { EPwm2Regs.TBPRD = PRD; // Set timer period EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0 EPwm2Regs.TBCTR = 0x0000; // Clear counter // Setup TBCLK EPwm2Regs.ETSEL.bit.SOCAEN = 1; //enable SOCA EPwm2Regs.ETSEL.bit.SOCASEL = 4; // Select SOC on up-count EPwm2Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW; EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; // Slow just to observe on the // scope // Set actions EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM2A on Zero EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; EPwm2Regs.AQCTLB.bit.CAU = AQ_SET; // Set PWM2A on Zero EPwm2Regs.AQCTLB.bit.CAD = AQ_CLEAR; // Active Low complementary PWMs - setup the deadband EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL; EPwm2Regs.DBRED = 100; EPwm2Regs.DBFED = 100; // Interrupt where we will modify the deadband EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT EPwm2Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event } void InitializeADC() { // Configure ADC AdcRegs.ADCMAXCONV.all = 0x0001; // Setup 2 conv's on SEQ1 AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; // Setup ADCINA3 as 1st SEQ1 conv. AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x2; // Setup ADCINA2 as 2nd SEQ1 conv. AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;// Enable SOCA from ePWM to start SEQ1 AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS) }