This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to GET RX PARAMETER on PHY_G3_EXAMPLE

Hi everyone,

I have some trouble to understand how does the PHY_rxGet(UINT16 getType, UINT16 *getData_p) works. I have implemented this function inside the code by first declaring the structure -> PHY_rxGetData_t rxget and then recall the PHY_rxGet function for example in this way:

-PHY_rxGet(PHY_RX_GET_TONEMAP_INFO,&rxget);

val10=rxget.toneMapInfo;

-PHY_rxGet(PHY_RX_GET_NL,&rxget);

val7=rxget.nl;  etc...

The problem is that when I look the variables: val10, val7 (that I have declared before as UIN16) the result is 0. Only If I put inside the function "PHY_RX_GET_TONEMASK" correspond with the TX value, but for example if I want to know the SNR or other parameter the value is always 0.

Can someone tell me the reason?

Thanks for your support,


Best,

Andrea