This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to allocate Flash memory to store data of array of large size in TMS320f28377d

Other Parts Discussed in Thread: CONTROLSUITE

Hi,

I am trying to allocate an array of large size in the flash by using pragma directive and assigning a section "myvars1" in the .cmd file. While compiling, there are no errors, but I am not able to assign any value to it , the variable shows 65535 value and any change to that value isn't happening. I am able to assign in a similar way to RAM but not to Flash. What might be the reason for that? Can we not assign Flash for storing data? Below is my cmd file. Any help on this would be appreciated. Thanks.

MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMLS5 : origin = 0x00A800, length = 0x000800

RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x0D000 // 53248
// RAMGS2 : origin = 0x00DCB0, length = 0x00C350 // 50000

/*
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
*/

CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}


SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0
.pinit : > FLASHB, PAGE = 0
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0

/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1

/* Initalized sections go in Flash */
.econst : >> FLASHF | FLASHG | FLASHH PAGE = 0
.switch : > FLASHB PAGE = 0

.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

.sysmem : > RAMGS1

// Filter_RegsFile : > RAMGS0, PAGE = 1


/* SHARERAMGS0 : > RAMGS0, PAGE = 1
SHARERAMGS1 : > RAMGS1, PAGE = 1
*/

/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}

myvars1 : >> FLASHA PAGE = 0

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

  • Priti Chakraborty,

    1) Try declaring the array as const.  See below example.

    #pragma DATA_SECTION(TrialBuffer,"TrialBufferSection");
    const uint16 TrialBuffer[8] = {0x1111, 0x2222, 0x3333,0x4444, 0x5555, 0x6666, 0x7777, 0x8888};

    2) Regarding your comment on editing the Flash contents:  In your application, if you want to edit the Flash contents, you need to use the Flash API.  See the example at C:\ti\controlSUITE\device_support\F2837xD\v190\F2837xD_examples_Dual\flash_programming.

    Thanks and regards,
    Vamsi

  • Thanks for the reply.But, I cannot define the array to be constant as I need to store the data obtained from analog to digital converter which will be obtained at run-time. Is there any other way to store the data obtained from ADC directly to flash as the RAM provided in the processor is limited.

    Regards,

    Priti Chakraborty

  • Priti Chakraborty,

    You can embed the Flash API in to your application and program the Flash at run time as you get data from ADC.

    Did you go through the Flash programming example that I referred?

    Thanks and regards,
    Vamsi

  • Priti Chakraborty,

    Hope you are able to program Flash using Flash API.
    I am closing this thread for now. You can re-open this thread if you need any help or you can start another thread.

    Thanks and regards,
    Vamsi