Other Parts Discussed in Thread: SFRA
Hi,
I am working on the implementation of a power converter with digital compensantion by means of SFRA library. I found that the DPS workshop example code (fixed point for TMS320F28025) has pretty much everything I need to get started with the Library. However, I don't have the DPS workshop kit, instead I have the Piccolo F28025 Control Card with the Docking station.
Here's my situation: If I try to debug the original code, it works just fine in the sense that I can see expressions' values changing in real time without debbugging issues. I haven't tried to connect any circuit, though.
However, since I didn't want to overwrite the existing code, I created a copy of it (exported and imported it with another name). This has caused me a lot of issues because the project configuration was lost (building and linking sources, debug configuration, etc.).
After dealing with the mentioned issues I was finally able to run the code and start debugging. Now, it works just fine until it gets into "ADC_SOC_CNF(...)" function call. Specifically the problem is "DSP28x_usDelay(1000)" call inside ADC function.
When it tries to execute the call, something triggers the CPU to execute the assembly instruction "ESTOP", which apparently halts the CPU.
I noticed that there's another function called DELAY_US(A) inside of "DSP2803x_Examples.h" and that I had used for the DC Event trip with the comparator example code. So, I tried to include that header file into my project, but the compiler throws an error due to different definitions of symbols:
RamfuncsLoadStart;
RamfuncsLoadEnd;
RamfuncsRunStart;
inside "DSP2803x_GlobalPrototypes.h", which is included into "DSP2803x_Examples.h", and {...}-Main.c
I also noticed that most headers and .asm files included in the project were copied as simple files and aren't linked as they are in the original project.
So, I tried by erasing "DSP2803x_usDelay.asm" and adding it by hitting right-click on project > add files... > path > Link to files & and relative to PROJECT_LOC. However, nothing changed.
I am wondering what is it that its causing so much troubles if the codes are essentially the same. I think it has to do with the non-linked files.
I will really appreciate any help you all can bring me on this.
Regards