Dear Supplier,
I'm using Code Composer Studio Version: 6.1.2.00015 and DPLibv3_4Template-F2803x to develop my firmware.
1- In Project Explorer I'm performing COPY of the project DPLibv3_4Template-F2803x, PASTE and RENAME.
2- I run the copied project and it works well.
3- I perform changes in the original code to perform tasks according to my application: ADC configuration, PWM etc...
4- I test the modified code and my code works well.
5- I close code composer studio and restart my laptop.
6 - I open code composer studio and run my project (the same that was working before closing CCS), the following problem happens:
Trouble Reading Register PC: (Error -1142 @ 0x0)
Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.
(Emulation package 6.0.407.3)
0x3FF599 (no symbols are defined for 0x3FF599)
7 - I run again the original project DPLibv3_4Template-F2803x without my changes and it works well.
8 - I run my modified project and it runs correctly.
What could be the reason for this problem?