Hi,
I just recently got a LaunchPad product (LAUNCHXL-F28377S), and am trying to output on the DAC channels. I've successfully been able to read in through the ADC channels which from what I understand from a similar post are muxed into the same pins, and have also tried using the sample code "buffdac_enable_cpu01" on all three DAC channels (i.e., DACA, DACB, and DACC). I've been reading the voltage on pins 27, 29, and 24 against ground but can't seem to get anything but a zero voltage. Are these the correct pins? Is there something I'm missing?
Thanks!