This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please build the binaries for AT91RM9200 microcontroller.
Now I use ".\SW\bin\OMAP\prime_dc" from "PrimeDC_SDK_PackageV3600"
And there is a problem.
Total nodes ~300. The program crashes after a good work for 2 days:
Sep 30 10:19:31 ucdk Prime Base Node: <COMM_dspKeepAliveRespHndlr> attempts curr<1> / total tx<711>/rx<711> Sep 30 10:19:31 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump ---------------- Sep 30 10:19:31 ucdk Prime Base Node: UTIL_genStackTrace - 1 : [0x41988d94] Sep 30 10:19:31 ucdk Prime Base Node: <UTIL_genStackTrace> -------------------------------------------------
The program works fine and stable if the nodes ~100.
Hello Elizabeth,
I have no installation package "PrimeDC_SDK_PackageV3600.exe", but already have installed SDK at "c:\Texas Instruments\PrimeDC_SDK_PackageV3600".
Inside installed SDK i see dc binaries:
"c:\Texas Instruments\PrimeDC_SDK_PackageV3600\SW\bin\AM335x\prime_dc"
"c:\Texas Instruments\PrimeDC_SDK_PackageV3600\SW\bin\OMAP\prime_dc"
I was sure that these binaries can be found in TI-PLC-PRIME-DC v4.0.0.0.
Should I download the controlSUITE ? (~1.7Gb)
Thanks,
Victor
Hi MEGHANA MANAVAZHI
I have binaries "c:\Texas Instruments\PrimeDC_SDK_PackageV3600\SW\bin\OMAP\prime_dc"
As I understood, this binaries are for OMAP-L13x processors.
YES, I run this binaries on AT91RM9200 processor (with Linux).
Now, I'm just looking for modern version binaries ("TI-PLC-PRIME-DC v4.0.0.0"...\OMAP\prime_dc).
Best regards,
Victor
The new program also displays the "assert" and unloaded from memory.
Oct 19 21:10:29 ucdk Prime Base Node: <NWM_regTimerStart> Entry ... Oct 19 21:10:29 ucdk Prime Base Node: <NWM_regTimerStart> Exit ... Oct 19 21:10:29 ucdk Prime Base Node: <CNM_connEstRespHndlr> Entry ... Oct 19 21:10:29 ucdk Prime Base Node: <MP_SBM_pool_free> SBD <0x8ea8c> freed Oct 19 21:10:29 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BD <14282> Oct 19 21:10:29 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BUF <4750> Oct 19 21:10:29 ucdk Prime Base Node: <UTIL_genStackTraceMsg> --------------- assert stack dump ---------------- Oct 19 21:10:29 ucdk Prime Base Node: 19-09-16 21:10:29.875 [1413] assert: PDC: Signal SIGSEGV: 11 Oct 19 21:10:29 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump (cnt<2>) ---------------- Oct 19 21:10:29 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump ---------------- Oct 19 21:10:29 ucdk Prime Base Node: UTIL_genStackTrace - 1 : [0x4219b9d4] Oct 19 21:10:29 ucdk Prime Base Node: <UTIL_genStackTrace> ------------------------------------------------- Oct 19 21:10:29 ucdk Prime Base Node: <UTIL_genStackTrace> ------------------------------------------------- Oct 19 21:11:03 ucdk Prime Base Node: Initializing ....
Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> SBD <0x94210> freed Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BD <14280> Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BUF <4748> Nov 1 12:28:38 ucdk Prime Base Node: <NWM_Reg_TX_Msg_B> Exit ... Nov 1 12:28:38 ucdk Prime Base Node: <NWM_regTimerStart> Entry ... Nov 1 12:28:38 ucdk Prime Base Node: <NWM_regTimerStart> Exit ... Nov 1 12:28:38 ucdk Prime Base Node: <CNM_connEstRespHndlr> Entry ... Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> SBD <0x94060> freed Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BD <14281> Nov 1 12:28:38 ucdk Prime Base Node: <MP_SBM_pool_free> N of free BUF <4749> Nov 1 12:28:38 ucdk Prime Base Node: <UTIL_genStackTraceMsg> --------------- assert stack dump ---------------- Nov 1 12:28:38 ucdk Prime Base Node: 01-10-16 12:28:38.319 [850] assert: PDC: Signal SIGSEGV: 11 Nov 1 12:28:38 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump (cnt<2>) ---------------- Nov 1 12:28:38 ucdk Prime Base Node: <UTIL_genStackTrace> --------------- assert stack dump ---------------- Nov 1 12:28:38 ucdk Prime Base Node: UTIL_genStackTrace - 1 : [0x4219b9d4] Nov 1 12:28:38 ucdk Prime Base Node: <UTIL_genStackTrace> ------------------------------------------------- Nov 1 12:28:38 ucdk Prime Base Node: <UTIL_genStackTrace> ------------------------------------------------- Nov 1 12:29:12 ucdk Prime Base Node: Initializing ....