Hello all,
I m trying to activate CPU2 to exchange data with CPU1 by IPC and send via SCI.
CPU1 code is working from FLASH.
CPU2 code is working from RAM.
I would like to have also CPU2 code executed from FLASH. I extracted the project example "dc_blinking _cpu2". The LED is blinking from RAM, but i have an error when trying to debug from FLASH.
From another POST i have assumed i have to set my CPU1 code to "CPU1_FLASH_STANDALONE". Can you povide me how i can import this build setting into my existing project which does not have this build setting?
What am i supposed to do then to have CPU2 code running from FLASH ?
Thank you!
Thank you!