Tool/software: TI C/C++ Compiler
As we know the data type 'int' is different between CPU and CLA, this cause some problems in my program:
Like I defined a 'int' variable in a cla source file and declared it in the corresponding header file and expected it to be shared with CPU, while, the CPU will see this 'int' variable differently.
Also, If peripheral like epwm is going to be accessed in the cla program, usually the 'F2807x_device.h' should be included, but the variables in these header files are declared by the CPU types rather than CLA type, which may cause error as well, even whe i did this the compiler told me this:
Description Resource Path Location Type
#452 the type "long long" is nonstandard F2807x_device.h /GenericDrive_CLA/HAL/Driver/F2807x_headers/include line 132 C/C++ Problem
#452 the type "long long" is nonstandard F2807x_device.h /GenericDrive_CLA/HAL/Driver/F2807x_headers/include line 135 C/C++ Problem
#838 unrecognized cregister name 'IER' F2807x_device.h /GenericDrive_CLA/HAL/Driver/F2807x_headers/include line 32 C/C++ Problem
#838 unrecognized cregister name 'IFR' F2807x_device.h /GenericDrive_CLA/HAL/Driver/F2807x_headers/include line 31 C/C++ Problem
Any way to work this around? Any comments are appreciated!