Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Dear Ti community,
I'm develop a peak current mode control on a phase shifted full bridge. My configuration for EPwm1 & EPwm2 is nearly the same as on the HVPSFB evaluation board software. Also the principle for the phase modification depanding on the comparator output is the same.
Through my understanding it is not possible that at a set value iref = 0 the phase of the two pwms is exactly zero. => When i set the set value iref = 0, i have a little overlap of the diagonal switches and the output
on the secondary side of the transformer is not zero.
Because the Action Qualifier Register of EPwm2 toggle at zero between NOTHING and FORCE TO ZERO.
Is my understanding right?
Thank you for your answer,
Best regards
Tobias