This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28027: How much is the minimum Power Consumption of TMS320F28027F

Part Number: TMS320F28027


Tool/software: Code Composer Studio

How much is the minimum Power Consumption  of  TMS320F28027F ?   Download  Example_F2802xHaltWake into the TMS320F28027F;   the current measured is 5mA.

The power supply system with   TPS54061,Power in 24 V power supply,  Current Consumption have 256uA.(there is No load)

The entire board welding with a minimum system, and a download the circuit. Runninng Example_F2802xHaltWake ,the Current Consumption is 5mA,and then wake up the Current Consumption is 10mA.

How much is the minimum Power Consumption of  TMS320F28027F? Could I reduce it more?