This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Problem with ADCIN A2/A3/A4 + documentation

Part Number: LAUNCHXL-F28379D


I'm using the analog inputs A2, A3, A4 and A5 from the LauncXL-F28379D, for convenience all of them are connected to GND over an 1 kΩ resistor. All inputs are configured as an 16 bit input.
Now there are 3 different situations.

A5: Works fine, with voltages from 0 V up to 3.3 V.

A3+A4: The voltage at ADCIN is GND, but the result register contains 65510 ... 65535, mostly 65535. Another voltage will change nothing.

A2: The output of the OPAMP is 0 V (OK), at the ADCIN there is 3.0 V (not 3.3 V). The AscResult says 0 ... ~20. Another voltage will change nothing.
If I disconnect the LauncXL completely from my board, the voltage falls to 0 V (µC and my board). If i only disconnect te connection to the OPAMP, then at the ADCIN there are still 3.0 V.
The LaunchXL User's Guide shows that there is only a connection to the µC. That means the 3.0 V comes from the µC. But it is inconsistent at this point. For U16 there is written "ADCINA2/CMPIN1P" (input only), the signal name is "ADCINA2/ANALOGIN" (input only), but at J3 it's "Analog Out/I2S DO" (output!).

Thanks for help!

Edit: The reason was 16 bit while using single mode und the usage uf ADC A2.

Here is the configuration of the ADCA:

EALLOW;
EPwm9Regs.TBPRD = 2603;
EPwm9Regs.TBCTR = 0;
EPwm9Regs.TBCTL.bit.HSPCLKDIV = 0;
EPwm9Regs.TBCTL.bit.CLKDIV = 0;

EPwm9Regs.ETSEL.bit.SOCAEN = 1;
EPwm9Regs.ETSEL.bit.SOCASEL = 1;
EPwm9Regs.ETPS.bit.SOCAPRD = 1;

PieVectTable.ADCA1_INT = &adca_isr;
AdcaRegs.ADCCTL2.bit.PRESCALE = 2;
AdcSetMode(0, 1, 0);
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;

DELAY_US(1000);

AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1;
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;

AdcaRegs.ADCSOC0CTL.bit.CHSEL 	= 3;	
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 21;
AdcaRegs.ADCSOC0CTL.bit.ACQPS 	= 511;

AdcaRegs.ADCSOC1CTL.bit.CHSEL 	= 2;
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 21;
AdcaRegs.ADCSOC1CTL.bit.ACQPS 	= 511;

AdcaRegs.ADCSOC2CTL.bit.CHSEL 	= 4;
AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 21;
AdcaRegs.ADCSOC2CTL.bit.ACQPS 	= 511;

AdcaRegs.ADCSOC3CTL.bit.CHSEL 	= 5;
AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = 21;
AdcaRegs.ADCSOC3CTL.bit.ACQPS 	= 511;

EPwm9Regs.TBCTL.bit.CTRMODE = 0;

EDIS;

PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
IER |= M_INT1;
  • Hi Terence,

    There is an errata for the LaunchPad where A2 is connected to VREFHI = 3.0V:
    e2e.ti.com/.../581950

    For the other channels, if you are using 16-bit mode you need to provide differential inputs to the ADC. If the VREFHI is 3.0V and you connect 2.9V to the + input and 0.1V to the - input, then the expected output is 65536*(2.9 - 0.1 + 3.0)/(2*3.0) = 63351

    For the differential inputs, the common mode should be within 50mV of VREFHI/2. The common mode for 2.9V and 0.1V = (2.9 + 0.1)/2 = 1.5V = exactly VREFHI / 2.

    If you are using the A4/A5 channel pair, setting the channel select to 4 or 5 will produce the same result (a sample of A4/A5).
  • ADC B0 and B1 are also affected. The most powerful and the most unlucky board, hard to compile (linking), sometimes freezing in debugging due to activation of real-time debug mode for two cores concurrently.