Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE, TMS320F28335
Tool/software: Code Composer Studio
Hi,I am using f28069 launch pad to run PMSM .I want to work on sensor-less motor control.I should have good below 10 % base speed and above 10 % base speed control.I searched for the lab modules available in motorware.I have 2 questions.
1.Can I get a code(any lab module) for sensorless Motor control+Kalman filter.If yes ,suggest me the path
2. Is it necessary to use some high end controller(like TMS320f28335) when i go for Kalman filter?
Thank-you in advance.