This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320F28376D: TMS320F28376D

Part Number: TMS320F28376D


Tool/software: TI-RTOS

Hi,

I am having trouble getting CPU2 to boot properly.

CPU1 properties:

CPU2 properties:

Process:

Connect to CPU1.

Connect to CPU2

Load CPU2

Load CPU1

This is the only way I can get round the following error.

target configuration is:

After loading CPU2:

After loading CPU1:

Then I 'Suspend' CPU1:

I have tried several combinations of target configurations using the options in the target configuration 'Program/Memory Load Options' selections.

There should be a way to accomplish the loading and executing the two cores without going through this precise procedure.

As you can see, I am trying to run SYS/BIOS on both cores.

I can load and execute just CPU1 without problems.

Suggestions ?