Other Parts Discussed in Thread: MOTORWARE
I am working with motorware 14 and I want to use sensor feedback.
I am using lab 12b and I have connected encoder speed output as feedback. There is no problem at that stage, everything works fine with this. My question is the minimum speed that I can run the motor.
This is a 4-pole ACIM and my current loop works at 10 kHz and speed loop works at 1 kHz. I have a 1024 pulse incremental encoder. I want to control the motor down to 20 rpm. So that at every 1 kHz I will have 1024*4*20/(60*1000) = 1,365 increments at encoder module. I think it seems too low.
As a result what is your recommendation for the frequency of speed control loop at such a low speed?
Moreover, I want to check also if there is a problem with the encoder signals. For an example, if encoder is not connected or if A and B signals connected oppositely etc. I want to detect it. Is there any mechanism in Instaspin software that I can check those type of errors in encoder?