This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Launchxl-F28069M configuration problem.

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: CONTROLSUITE

hi, i am working with a launchxl-F28069M recently, but there are some things that i still dont understand. In the launch guide it says that if the TRSTn (number 3 in S1) is in the down position it will not connect with the debugger, then i put in up position. when i charge a program, it loads correctly but if i reset the launchpad with the reset buttom it starts running the program demo, why? so my program its not saved in the launchpad?

Another thing is, in many source codes that im developing, i need to see some variables in use, as the procces is not time critical i choose to see by console using the "printf" instruccion, supported by C language, but it sends me an error in the 28069_RAM_lnk.cmd file, and i dont have any idea of why. why is that? i have to do any additional configuration?

All the helps are welcome, thanks and regards.

 

Eliomar Conde.