Part Number: TMS320F28069
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello guys,
I am using EVAL KIT FOR TMS320F28X. I am trying to implement PWM+ADC in my development board. ADC pins are not working on my development board. PWM is working on same development board.
My code:
//Configure ADC
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // ADC
AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; // Use internal bandgap
AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Power up band gap
AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; // Power up reference
AdcRegs.ADCCTL1.bit.ADCPWDN = 1; // Power up rest of ADC
AdcRegs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC
AdcRegs.ADCCTL2.bit.ADCNONOVERLAP = 1; // OVERLAPPING of sample is not allowed
for (i = 0; i < 5000; i++)
{
} // wait 60000 cycles = 1ms (each iteration is 12 cycles)
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; // create int pulses 1 cycle prior to output latch
//set S/H window to 6 clk cycles (112.5ns)
AdcRegs.ADCSOC0CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC1CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC2CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC4CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC5CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC6CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC9CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC8CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC10CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC12CTL.bit.ACQPS = 8;
AdcRegs.ADCSOC14CTL.bit.ACQPS = 8;
//AdcRegs.INTSEL1N2.bit.INT1SEL = 12; // ADCCH12 (ADC-B4) EOC causes ADCInterrupt 1
// AdcRegs.INTSEL1N2.bit.INT1CONT = 1; // set ADCInterrupt 1 to auto clr
AdcRegs.INTSEL1N2.bit.INT1E = 0; // disable ADC interrupt
//Note that SOC3, 7, 11, 13 & 15 are valid, but these SOCs are not configured
//since these ADC outputs do not exist on the controlSTICK. The configuration
//is configured as it is for readability.
//EOC = end of conversion event; SOC = start of conversion event
AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 0; // NO ADC intrrupt selected 1 causes SOC0
AdcRegs.ADCINTSOCSEL1.bit.SOC1 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC2 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC4 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC5 = 0;
AdcRegs.ADCINTSOCSEL1.bit.SOC6 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC8 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC9 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 0;
AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 0;
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 1; // ADC intrrupt is selected by CPU timer0
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC5CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC6CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC8CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC9CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC10CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC12CTL.bit.TRIGSEL = 1;
AdcRegs.ADCSOC14CTL.bit.TRIGSEL = 1;
//Select the channel to be converted when SOCx is received
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0; // convert ADC-A0 (CH0) when SOC0 is received
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; // convert ADC-A1 (CH1) when SOC1 is received
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2;
AdcRegs.ADCSOC4CTL.bit.CHSEL = 4;
AdcRegs.ADCSOC5CTL.bit.CHSEL = 5;
AdcRegs.ADCSOC6CTL.bit.CHSEL = 6;
AdcRegs.ADCSOC8CTL.bit.CHSEL = 8;
AdcRegs.ADCSOC9CTL.bit.CHSEL = 9; // convert ADC-B1 (CH9) when SOC9 is received
AdcRegs.ADCSOC10CTL.bit.CHSEL = 10;
AdcRegs.ADCSOC12CTL.bit.CHSEL = 12;
AdcRegs.ADCSOC14CTL.bit.CHSEL = 14;
EDIS;
Can you guys please help me out here?
Regards,
Ranjit Chennamchetty