Part Number: TMS320F28069
I am developing a project based TMS320F28069. I am facing very strange issue. In the following code snippet- I am receiving data rxCmdPkt.recvpkt.EpcData = 0x31 from a remote system. I am able to print the same in a hyper terminal in the following lines
scia_xmit(0x44);
epcmd=rxCmdPkt.recvpkt.EpcData;
scia_xmit(epcmd);
But the serial print inside if loop and switch loop are not working
void epccmdProcRRtask(void)
{
// char epcmd;
if(newCmdAvlbl())
{
rxcmd=retrieveCmd();
rxCmdPkt.recvpkt= rxcmd;
// ROM_UARTCharPutNonBlocking(UART0_BASE, rxCmdPkt.recvpkt.EpcData);
scia_xmit(rxCmdPkt.recvpkt.StartByte);
scia_xmit(rxCmdPkt.recvpkt.MsgID);
scia_xmit(rxCmdPkt.recvpkt.EpcData);
scia_xmit(rxCmdPkt.recvpkt.Checksum);
scia_xmit(rxCmdPkt.recvpkt.EndByte1);
scia_xmit(0x44);
epcmd=rxCmdPkt.recvpkt.EpcData;
scia_xmit(epcmd);
if(epcmd == 0x31)
{
scia_xmit(0x45);
XmitMessage(rxCmdPkt.RxMsgArray, 5);
}
// scia_xmit(epcmd);
switch(epcmd)
{
case 0x31:
scia_xmit(0x45);
XmitMessage(rxCmdPkt.RxMsgArray, 5);
// setEpcStsXmitRequest();
break;
case EpcHeaterON:
epcHeatON(rxCmdPkt.recvpkt);
break;
case EpcHeaterOff:
epcHeatOFF(rxCmdPkt.recvpkt);
break;
case EPCForceModeON:
epcForceModeONfn(rxCmdPkt.recvpkt);
break;
case EPCForceModeOFF:
epcForceModeOFFfn(rxCmdPkt.recvpkt);
break;
case EPCTXON:
// ROM_UARTCharPutNonBlocking(UART0_BASE, EPCTXON);
XmitMessage(rxCmdPkt.RxMsgArray, 5);
epcTXON(rxCmdPkt.recvpkt);
break;
}
}
}
The optimizaton is OFF
Could you help
Regards,
Ramesh