This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi all,
The customer has very strict requirements on system clock. They tested the 28035 using internal crystal, there are few micro seconds error in one minute. There is a 10MHz crystal in 28035? I want to know the certain accuracy of the internal crystal?
It give the information about the frequency varied vs temperature. However, it didn't tell me the max frequency and the min frequency of the internal clock.
To elaborate a little more on this, the zero-pin oscillator is very temperature sensitive.
For the F2802x, F2803x, F2805x, F2806x series of devices, there is a temperature trim software sequence that can be executed to nudge the frequency back to about +/- 1.5% accuracy for the temperature at which the trim is executed. The trim sequence needs to be executed periodically (as frequently as the temperature is expected to change) in order to keep it in the +/- 1.5% range.
The F2807x and F2837x devices do not have a software trim sequence. Instead, the oscillators are continually kept within a +/- 3% range using analog circuitry. This eliminates the overhead of software trimming, but also widens the trimmed error range.