Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Dear,
Hi, I'm trying to use CLA for simple calculation(normalisation, etc) with ADC results, and this is the first time that I use CLA.
Initialisation, configuration of CLA RAM in main seems fine, but I encounter a problem when I add '.cla' file on my source code.
The error statements are following:
#35 #error directive: "Header file <stdio.h> not supported by CLA compiler"
#452 the type "long long" is nonstandard.
.cla file contains cla tasks interrupt functions which cla are using.
I added 'CLA_C=1' on C2000 Linker -> Advanced Options -> Command File Preprocessing -> Pre-define preprocessor macro.
I set cla1 as 'specify CLA support'.
Is there any solution for this problem? If you need more information, I'll reply to this post