Part Number: TMS320F28034
Hi,
my customer is using F28034, and the SYSCLK is set as 60MHz, XCLKOUT output is 15MHz to be measured.
when they do EFT test, they will observe XCLKOUT to be 7.2MHz and the PWM frequency change, which means the SYSCLK is changed.
When they remove the EFT pulses, the clock is still wrong.
They are using internal oscillator as the clock source, so they suspect that the internal oscillator is too easy to be influenced and caused the failure of EFT test.
I will check with the customer to see if the power(3.3V, 1.8V) is within our recommendation range during EFT test, but I don't consider power is the reason, because the clock is still wrong when they remove the EFT pulses.
Do you have any idea what else might be the reason for the wrong clock frequency?
Howard