This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Is memory utilized if it's not specified in the *.cmd linker command file?

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

If a section of memory is not specified in the command linker file's MEMORY section will it be inaccessible during the linking process?

For example:

MEMORY
{
    /* Mx is MCU dedicated */
    RAMM0       : origin = 0x000121, length = 0x0002DE
    /*RAMM1       : origin = 0x000400, length = 0x0003FF*/
}

If RAMM1 is commented out what is the net effect during the linking process and at run-time?

Kindly,

Graham