I have configured the 2 HRPWM A channels for high resolution period mode (I try to control the frequency keeping 50% pulse width). The channels are in sync and no jittering. But If I want to be sure that these two channels will be synced and enable the sync out from unit ePWM1 (CTR=ZRO) then there will jittering among the channels. If I use up count mode the jittering between channels is 1Tick=~17ns and if I use up-down count mode the jittering is 2Ticks. It seems so that the other channel looses it's high resolution mode when synchronizing from other ePWM unit, because the jitter is in Ticks and not in high resolution ticks (160ps or so). According to HRPWM manual if MEP controls the period it should be possible to control the phase and edge also, so this sync should work, right?