Other Parts Discussed in Thread: LAUNCHXL-F28379D
Tool/software: Code Composer Studio
Hi,
I am trying to compile "IDDK_PM_Servo_F2837x_v2_00_00_00" project in controlSUIT (C:\ti\controlSUITE\development_kits\TMDSIDDK_v2.0\IDDK_PM_Servo_F2837x_v2_00_00_00) by using LAUNCHXL-F28379D. I set the build level to LEVEL1 because I want to test the PWM outputs. Although I am able to see the SVGENDQ_MACRO outputs (duty cycles) as in mentioned in "Sensored FOC PMSM_IDDK_v2.pdf page 21", I cannot see the PWM output on the EPWM pins (for example pin40 (GPIO 0) on Launchpad).
I think same issue has been discussed in here "https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/577175" . However, problem remained unsolved in that post.
Any suggestion would be welcome.
Thank you,
Eray