Part Number: TMS320F28035
Other Parts Discussed in Thread: DRV8301, , CONTROLSUITE, MOTORWARE
Hello everyone,
I have somewhat of a general question. I am using the TMS320F28035 along with the DRV8301 to drive a BLDC motor. Due to my ignorance of how the ePWM modules were paired (ePWMxA amd ePWMxB), I had designed the board to use all ePWMxA's (ePWM1A-ePWM6A) for the PWMs sent to the DRV8301. Luckily, I learned from one of you guys at TI that it is possible to use complimentary PWM in conjunction with SVPWM techniques to control the motor. So I decided to do the following with what I had to work with:
1. I setup the DRV8301 to use 3PWM mode with default dead time (seems to be enough dead time now but may increase dead time later).
2. I am now using only ePWM1A, ePWM2A, and ePWM3A (I am letting the DRV8301 take care of the complimentary pwm signals).
3. I am using the built in current amplifiers of the DRV8301 to measure the phase currents.
4. Using the motor Hall signals to measure speed and rotor position.
So now for the question. Since I do not have any type of PI controller or anything else other than Hall signals and current measurements, how would I apply the information I am obtaining from the motor to implement SVPWM? My thoughts are that I can use the halls to determine what sector needs to be used. And then I can measure the current to determine the timing for the two space vector pwm settings along with the null vector pwm settings. I am trying to implement center aligned forward-reverse SVPWM. I understand the concept of SVPWM (I couldn't quit smiling when it clicked in my mind lol), but I have never implemented the SVPWM technique. In fact, this is my first time designing a motor controller. Also, just one more question about PWM: Is there a rule of thumb for how fast the PWM frequency needs to be? My MCU is running at approximately 16 MHz, and I heard that the PWM frequency should be at least 10x's the electrical frequency of the the motor. Any suggestions or help would be greatly appreciated.
Thank you,
Brandon