This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champion,
My customer find they use F28377D CPU1/2 erase download program to flash in their bootloader code need to decode password, then can do it, Their bootloader code is in FLASHA de LSRAM, all is secure RAM. They find in TMX version, it do not need password to do it. They assign D0, D1, LASRAM to zone1. Same code in TMX one is ok, but in TMS chip, bootloader code cannot operate FLASH if not inlock password.
Do you know we have change this function in TMS version one? In TRM, it say secure menory can operate serure menory not unlock.
Thanks!
BR
Joe
Hi Vivek,
I am also confuse why TMX version one can program without enable SEM bit, but TMS one need? Have you do this experiment ?
Thanks!
BR
Joe
Hi Joe,
Can you confirm if this issue is resolved after adding SEM in code.
Regards,
Vivek Singh