I am using Simulink Embedded Coder to program my microcontroller. I need to generate a 25kHz sine wave for my speaker.
I am monitoring the signal by connecting an oscilloscope to GPIO pin 70.
When the frequency is 25kHz there is no signal. The result is as follows:
Then I tested the system by reducing the frequency to 250Hz. The result is as follows:
Then I changed the step size from "auto" to 1/(5e5) and the result is as follows:
But as I said this signal disappears in about 100 seconds. In the video below, I captured this weird behaviour.
Why is this signal not continuous and it disappears after a while? Why does it not appear like a proper sine wave when the fixed step size is configured as "auto"?
Finally I will share some screenshots to help with the troubleshooting.
This is my code. First I generate a sine wave with Amplitude 1 and Frequency 250Hz. Then I amplify it by 2047 times and shift it up by 2047 in order to create a sine wave in the range of 0-2^12..
This is the configuration parameters window where I changed the Fixed-step size. Note the solver type is "Fixed-step" and Solver Type is "discrete (no continuous states)".