Part Number: TMS320F28069
Other Parts Discussed in Thread: CONTROLSUITE
Please tell me how should I keep PWM to low state on power ON. Even by pulling down pins and keeping pins to clear state some pins are remaining high on boot up.
Please help on how to configure ePWM1A for high from zero to CAU and ePWM1B high for PRD to CAD. I tried this and the settings are shown below, but I'm not getting the desired output. Please let me know if there are any changes to be made or should I use up mode for ePWM.
Please tell me how should I keep PWM to low state on power ON. Even by pulling down pins and keeping pins to clear state some pins are remaining high on boot up.
Please help on how to configure ePWM1A for high from zero to CAU and ePWM1B high for PRD to CAD. I tried this and the settings are shown below, but I'm not getting the desired output. Please let me know if there are any changes to be made or should I use up mode for ePWM.
// EPWM Module 1 config
EPwm1Regs.TBPRD = 2647; // 17kHz PWM @ 90MHz
// EPwm1Regs.CMPA.half.CMPA =2647/2;
EPwm1Regs.TBPHS.half.TBPHS = 0;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetrical mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // set actions for EPWM1A
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.PRD = AQ_SET;
EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR;
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
EPwm1Regs.DBFED = 10; //
EPwm1Regs.DBRED = 10; //
// Interrupt where we will change the Deadband
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 3rd event
// Disable EALLOW protected register access
//SOC Generation Setting // ADC start of conversion on period
EPwm1Regs.ETSEL.bit.SOCAEN = 1;
EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD;
EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST;
EPwm1Regs.ETSEL.bit.SOCBEN = 1;
EPwm1Regs.ETSEL.bit.SOCBSEL = ET_CTR_ZERO;
EPwm1Regs.ETPS.bit.SOCBPRD = ET_1ST;
// updating duty cycle in interrupt
interrupt void epwm1_isr(void)
{
EPwm1Regs.CMPA.half.CMPA = duty_cycle;
EPwm1Regs.CMPB = (duty_cycle);
// Clear INT flag for this timer
EPwm1Regs.ETCLR.bit.INT = 1;
// Acknowledge this interrupt to receive more interrupts from group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
need is to generate PWM 1A with duty cycle variable and PWM 1B with same duty cycle shifted by 180 degrees for full bridge converters.
Please help.