Part Number: TMS320F28234
Hello,
This is related to the thread "eQEP - Position Counter Reset on the First Index Event not available after SW reset". I find that the "Position Counter Reset on the first Index Event" mode of the PCCU in the eQEP module works as described, but only after a device reset. If, after the First Index Event has be acquired and the FIMF has been set, the eQEP peripheral is reset (QEPCTL.QPEN = 0) and/or the First Index Marker Flag has been cleared (EQep1Regs.QEPSTS.bit.FIMF = 1), the device will not reacquire the First Index Event.
Has this issue been confirmed as a bug and is there a workaround other than resetting the device?
Thanks in advance.