Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi All
I have a question about TMS320F28335. Recently we made 60 pieces of circuit board used TMS320F28335 as the main control chip. We found 10 pieces of circuit board couldn't download .out file to the chip. The schematic circuit diagram is a mature scheme, has already produced many batches, have not encountered such problems before, and all the circuit board made used the same schematic diagram. Due to the shipping demand, we replaced the main chip on the problem board with a new chip. Then everything was alright.
We left one piece of problem board for exception analysis.
We also resolder the welding if the welding is not good. But the problem is still there.
We do some test on input voltage 3.3V,1.8V and the external crystals signals. All the signals we tested is all right, the screenshot is shown as below.
The version of CCS we used is 3.3. Can you give me some advise on how to lock possible problem points? Thanks a lot.