Part Number: TMS320F28335
Hi Team,
There's an issue from the customer need your help:
Pass the parallel data to the address 0x04000 through AD7606 (although the data cannot be passed in). When the DSP address reads this address, the DSP will report Trouble Reading Register PC:(Error -1156 @ 0x0)Device may be operating in low- power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device.(Emulation package 9.2.0.00002) .
Thanks & Regards,
Ben