Part Number: TMS320F28052F
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
I need to be able to perform a DFU to my TMS320F28052F through a serial connection (RS-485) using pins 49 and 48 (which correspond to GPIO7 and GPIO12 respectively).
The initial approach was to boot the device in SCI mode and use controlSUITE/C200Ware's serial_flash_programmer utility, but when the device boots into SCI, the mapping of the pins for SCIRXDA and SCITXDA are to their respective locations at pins 41 and 42. These pins are currently used as SCLA and SDAA ports.
It has been suggested to me to keep the SCI kernel (which I assume is the .txt file found when compiling the example project from C:\ti\controlSUITE\device_support\f2805x\v104\F2805x_examples_ccsv5\f28052f_flash_kernel) in flash, then copying it to RAM while the device is in a regular boot mode, then executing the programmer using pins 48/49.
I've viewed some related threads to this subject:
https://e2e.ti.com/support/microcontrollers/c2000/f/171/p/155583/681411#681411
However, under controlSuite/C2000Ware's libraries, there are no boot_rom sources for me to reference (as it was mentioned in above threads).
I guess my initial questions are as follows:
-What portions of a code would I need to edit/include to enable branching to SCI boot but maintaining the "regular" boot pin map?
-Once the SCI kernel is saved to flash/code edited as needed, how would I implement the serial_flash_programmer with this new setup?
This is all pretty unfamiliar territory for me, so any insight or direction would be much appreciated,
James