This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
I want my CPU2 application to run on GSxRAM of my F28379D. So , I modified the RAM.cmd file and placed .text into GSxRAM. However, when I try to load the program using JTAG, it doesn't work. It is because first I have to assign GSxRAM to CPU2 using GSxMSEL registers. And this process should be done by CPU1. If I move .text to LSxRAM of CPU2 instead of GSxRAM, everything works fine. However my .text size will be much more than all LSxRAM of CPU2 and I will need to use GSxRAM as well.
My question is, is there any other way that we can assign GSxRAMs to CPU2, so that there is no need to load a program to CPU1 for the assignment?
Regards,
Hakan
Hi Hakan,
If you don't want to run the CPU1 application then you can modify CPU1 Gel file (right click on CPU1 target and open Gel file) and add the code inside OnReset() or OnConnect() function to allocate GSxRAM to CPU2. This will work as long as you connect to CPU1 in CCS. But in standalone mode you have to have CPU1 code to assign GSxRAM to CPU2 and only after running that you can run CPU1 code.
Regards,
Vivek Singh