Part Number: TMS320F28377S
About example 2837x_vcu2_cfft_128 ,ask a few question.
1.the result of data_output.h are inconsistent with the matlab calculation
2.What is input data format? is it Real+image? or image+Real?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377S
About example 2837x_vcu2_cfft_128 ,ask a few question.
1.the result of data_output.h are inconsistent with the matlab calculation
2.What is input data format? is it Real+image? or image+Real?
thanks.
Hi,
The input is Re + Imag. I tried the following in MATLAB and got the same magnitude plot
A = [ copy all data from data_input.h here] ; data = reshape(A',1, 32*8); input = data(1:2:256)+data(2:2:256).*i; input(1); % should be 2232 + 1930i spec =fft(input); spec_mag = abs(spec); B = [ copy all data from data_output.h here] ; gold = reshape(B',1,32*8); gold_complex = gold(1:2:256)+gold(2:2:256).*i; sp(1)=subplot(1,2,1), plot(abs(spec_mag)/128); sp(2)=subplot(1,2,2), plot(abs(gold_complex)); title(sp(1), 'MATLAB FFT'); title(sp(2), 'GOLDEN OUTPUT');
And i get the following figure
As for the complex spectrum, there are bound to be differences on account that MATLAB does a double precision computation while the VCU does 16-bit fixed point arithmetic.