Part Number: TMS320F280049C
Hi
I was wondering if it is possible to sync one ePWM module based on the action of another ePWM (NOT based on phase control register or ePWMxSYNC signals). For example, when ePWM1A goes LO, set ePWM2A HI. Reason being - ePWM1 is the master and its configuration changes cyclically, both A and B are used with active high complementary, and gets terminated by a external signal similar to peak current mode control. Then I have ePWM2 that I want to be synched to when ePWM1 is terminated. I can't just use ePWM1 period to generate SYNC signals on ZERO, CMPB, etc, since the termination time is not predefined internally.
I could just replicate the configuration within ePWM2, but I am hoping there is an easier way to do it, since the setup of ePWM1 uses a lot of peripherals, and would create a lot of duplication I am hoping to avoid.
Thanks
EPWMxSYNC