This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I would like to use the greatly featured F28069M and InstaSPIN-MOTION for designing 8 different types of servomotor drives.The servomotors are of 3-phase stator, brushless 8-to-10 poles rotor with integrated incremental encoder and electromagnetic brake. The servomotor rated voltage and DC link voltage is 350 Vdc.
For this application I am planning to design a single type of control PCB for all servomotor drives despite of the motors power variations and for each servomotor I am going to use the appropriate isolated gate driver and power switches (and peripherals) on another PCB according to each motor power rating.
You are kindly requested to;
1- Advise if I have chosen the best device for this application.
2- Advise the best and appropriate road map achieving my purpose.
3- Advise if I can program every and each control PCB based for each application using the USB and the JTAG emulator completely and tune each controller with the relevant servomotor.
4- Advise if I am going to need any other requirements.
Best Regards;
Adel Najafi