Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: MOTORWARE
When I use ,I am able to run the motor at 35K rpm but motor temperature reaches up to 50 degree Celsius in 10-15 mins.(using Lab 10a)
We have another bldc motor controller which makes it run for the same speed and the temperature doesn't go above 42 degrees.
What can possibly go wrong ? Is there anything I am missing in my code or I have not configured correctly?
'