Part Number: TMDSSOLARUINVKIT
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
I would like to increase the inverter frequency from 50kHz to 100kHz or 200kHz. I have modified "#define INV_FREQ 50000.0" to "#define INV_FREQ 100000.0" in SolarMicroInv-Settings.h, but it doesn't work. May I know what are those parameters changed in the code? Thanks.