This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28035: flash learning

Part Number: TMS320F28035


Tool/software: Code Composer Studio

hi

I am using this path code C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVPM_Enhanced_Sensorless_2803x

Actually I want to rewrite flash size that means I am assigning morethan 10 arrays(are int data type) with size 100 in the main file at globally

when I compile this file I am getting the error "program will" that error shows '.ebss' has exceeding the size limit(4096 bytes) then I read what is .ebss and I came to know that is for all globally declared variables.

Now how could I add more size to that .ebss without any address change of already declared variables.

please tell how to add flash size to a particular section

and also give me any flash adding example data without change the address of already declared variables.

thank you