Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE
Hello,
We use TMDSHVMTRPFCKIT to run a sensorless BLDC motor. Control card is using TMS320F28035 non isolated emulator. When we use the GUI (HVMTRPFCKIT-BLDC-GUI.exe) with the .out file provided by TI ( HVMTRPFCKIT-BLDC-GUI.out), the motor runs and the red LED on the control board(LD3) is blinking. However, when we use the .out file generated from the project files provided by TI ( HVBLDC_Sensorless ), the red LED stays on all the time( no blinking anymore) and it won't connect to the GUI anymore. in the project file. the file related to RAM is commented out and we build to FLASH. Also, the BUILDLEVEL is set to LEVEL6. What are we missing here? Highly appreciate your urgent response.
Thank you!