Part Number: TMS320F28377S
I have a trouble with endat 2.2
Currently I use chip TMS320F28377S for my project. But when I connect between 28377S vs Absolute Encoder Motor ( endat 2.2 standard), I just relized on TMS320F28377S (100pins) do not have GPIO6, 7 which the manual prefer to connect with MOTOR to create CLOCK (ENDAT_CLK and SPICLK).
Futhermore, When I wanna exchange GPIO6 and 7 by others pins but the lib providing by TI do not allow to access ( they default 2 pins 6 and 7 create CLOCK)
So WHAT I CAN DO NOW, IF I DON'T WANNA CHANGE CHIP.
AND, If someone has example code for endat 2.2, please can send it for me to refer ?
THANKS SO MUCH !