This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
customer wants to realise an FFT on the F28004x and ask for benchmarks. I send him the DSP FPU Lib document with the benchmarks inside. I think these benchmarks are done w/o TMU. Would this reduce the numbers? Do we have FFT benchmarks with TMU?
Regards, Holger
Edit: corrected version to 1.50
Holger,
Which version of the library is the customer looking at?
In version 1.50, the benchmark table indicates that the --tmu_support is enabled and some of the benchmarks have "TMU0" in the name. Note that the TMU won't impact all of the functions since it is only a few trigonometric operands. It will impact magnitude, phase, as an example.
Regards
Lori