Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: AMC1200-Q1, LM1117, C2000WARE
Hi you all,
Due to this post I have been question to my self how to achieve a clean signal into the ADC, a person in this post told us about the poor accuracy or stability? of the LDO in order to get a good clean reference voltage
I have been working with the LAUNCHXL-F28069M with a little sinusoidal signal provided by the AMC1200-Q1 and also I saw the spikes, and I used this configuration here:
So I'm wondering if there is a way to achieve more clean signals not affected by the LDO or the LM1117, or if there are some guidelines while designing voltages to the adc. Even if I do that design, I have to reference with gnd of the adc, What happen if the ground of the ADC is not ok?