Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hello,
when i flash the µC everything works fine and the programm run fine on the µc, but when i press the Button "Verify Image" i get this Error:
Verification failed: Values at address 0x82330@Program do not match Please verify target memory and memory map.
When I change in the cmd file the Allocate program areas and the initalized sections go in flash, than the error moves according with my memory/flash area changes.
When I look at this area at Uniflash memory read, I see for the complet area 0x82000 - 0x84000 in every sector 0000.
maybe the complet area is locked and Uniflash just can't compare because its not allowed to look in this area?
Best regards
Julian Dolderer