Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE,
Tool/software: TI C/C++ Compiler
Hey everyone,
I am trying to communication with PC over USB.
Actually, I am trying to understand the usb_dev_bulk example which located in C2000 examples (C:\ti\c2000\C2000Ware_1_00_06_00\device_support\f2837xd\examples\cpu1\usb_dev_bulk\cpu01).
Even I reconfigured the GPIO_Init routine (for LAUNCHXL-28379D, SCIA-RX: GPIO43, Mux val. 15 and SCIA-TX: GPIO42, Mux val. 15), still I can't get any messages but only 0x00 at the beginning. (By the way I worked on the sci_echoback example first and it works fine, I can read and write messages over USB connection)
Thanks for reading, any suggestions will be appreciated